2018-11-29 01:42 PM
I have generated a project in CubeMx and then opened it in truestudio. When attempting to compile and debug the project I receive this error complaining about my debug script (hmm). I've attached the server log.
The project is for a NUCLEO-L476RG board (and the project used the template for said board).
It appears line 106 to 114 shows that the STM32_Programer_CLI.exe program returns error code 1 "No debug probe" unfortunately the file STM32CubeProgrammer_a13268.log disappeared so I've no other clue. It does appear that the STLink is findable (see communication in log).
Is this an ST-LINK FW version issue conflicting with the STM32_programmer supplied with the CubeMX eclipse plugin?
Suggestions welcome thanks!