cancel
Showing results for 
Search instead for 
Did you mean: 

Failure at line 13 in Target software startup scripts

LPola.1
Associate II

Hello,

I use STM32F407 MCU and when debugging with Attolic True studio v 9.3.0 I SOMETIMES got following error:

Failure at line 13 in Target software startup scripts

Error finishing flash operation. I attach linker and startup files.

Any help will be appreciated it is really annoying!

Thank you

PS: I see that I am not only one with this problem

1 REPLY 1
Peter BENSCH
ST Employee

Atollic Truestudio is frozen at 9.3.0, no longer available and supported and and has been replaced by the free STM32CubeIDE, which can also import projects from Atollic. Maybe this is a way forward for you?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.