2018-10-04 5:13 AM
Hi, i'm facing the difficulty of compiling the HAL driver codes takes nearly a 1:30 -3:00 min. So what should i do now?:sad_but_relieved_face:. it is quite a long compilation time for my application.
@Community member
@Imen DAHMEN
2018-10-04 9:46 PM
@Community member it's works very well. it means a lot for me. thanks a lot.
i have another doubt . this hal file could make my mcu slow?? bacause of a bunch of file.
2018-10-04 9:48 PM
@Community member I'm using intel core i3 and windows 10.
i have an doubt if i'm using the ssd on my pc whether it will reduce my compile time or not??
2018-10-04 9:52 PM
@Community member sorry jack. i don't have any idea what you are talking about?
2018-10-05 12:00 AM
Keil has a batch build option for multicore systems. A lot of RAM helps, one of my primary systems has 8 cores and 48GB of RAM.
2018-10-05 12:17 AM
Have you disabled the "Browse information" generation, and did it help ?
> I'm using intel core i3 and windows 10.
> i have an doubt if i'm using the ssd on my pc whether it will reduce my compile time or not??
There is nothing that suggests such long compile times. You could still check the resource usage during compile time with the Task Manager. SSD over normal HD will not have a significant influence, at least from the second build on. Win FS's use to cache a lot of small files.
BTW, I'm with Jack. CubeMX is not really a premium choice for an embedded project.
My SPL-based builds (full rebuilds) use to take only a few seconds as well.
2018-10-05 1:19 AM
@Community member yeah it worked out well.
could you elaborate the SPL ??, because i'm totally beginner at this.
for me cubemx is not reliable for me. i'm try to build it from scratch but results "premature optimization is a root cause of evil" so i get depressed.