F427 - Timer interrupts right after start?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-11 2:46 AM
Hi Guys,
I am setting up my F427 with a master-slave timer (TIM4->TIM1). TIM4 triggers two capture and compare interrupts, CC2 (CCR2 = 1), and CC4 (CCR4 = 5000). TIM1 is triggered by CC2 signal. The behavior of the configuration is correct, unfortunately when I start the master-slave timer with:/* start slave-timer */
if
(IS_TIM_ADVANCED_INSTANCE(TimSlaveHandle.Instance) != RESET)
{
/* Enable the main output */
__HAL_TIM_MOE_ENABLE(&TimSlaveHandle);
}
/* Enable the Peripheral */
__HAL_TIM_ENABLE(&TimMasterHandle);
the interrupts are triggered right after. In this regard I found this link
https://electronics.stackexchange.com/questions/161967/stm32-timer-interrupt-works-immediately
. If I debug, the UIF and the UE flags are cleared, but I still get the interrupts of CC2 & CC4. If I read the manual right (p. 520), this is the correct behavior. Am I right? In other words, when I start my PWM counter it immediately triggers an interrupt? Thanks you for your time and help. eimer #interrupt #flag #updat #interrupt #stm32 #stm32 #timer #timer #timer- Labels:
-
Interrupt
-
STM32F4 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-11 3:43 AM
Generate update event by software before enabling timers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-11 6:39 AM
Hi life_augmented.st,
This is not an intrinsic issue; not related to Timer peripheral but related to the way
TIM_Base_SetConfig(..) function is coded (called in HAL_TIM_Base_Init(..) ).
In fact, this function sets the update generation bit ( UG) which sets the update interrupt flag UIF, and an update interrupt is generated.
If a user, in a case like yours, want to customize and disable the generation of interrupt when setting the UG bit with keeping it coming only from counter overflow/underflow source, he should enable the URS bit in the TIM_CR1 register before calling the Timer base Init function :
/* Set the URS bit */
TIM1-> CR1 |= TIM_CR1_URS;
/* Call Timer base Init */
HAL_TIM_Base_Init(..);
/* Reset the URS bit */
TIM1-> CR1 &= ~ TIM_CR1_URS;
-Hannibal-
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-13 4:29 AM
Hi Hannibal & dembek,
Thank you for your quick reply. Your fix works like a charm for the problem I stated. Unfortunately, my problem shifted now. The issue is now, after I started the master once, stop the timer, and start it again, the first pulse is not generated at all. Only the next (second) pulse is generated. This is a strange behavior to me. On the other hand, if I set the UG-bit, the behavior is the other way around. This is really confusing me...Thank you for your time and help, if anybody can point me in the right direction, that would be highly appreciated.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-13 6:57 AM
I need to take back what I said, I did make an mistake here.
Setting the URS-bit is not protecting the f427 to throw an interrupt for CC2 or CC4. In fact it is changing anything for me.On the positive side, if you want to resolve the issue with a pulse missing after a start-stop-start cycle, you simple need to reset the counter value of the timer. For me TIM4->CNT = 0.I hope somebody can help, this felt solved and then the problems popped up again :(