2016-09-09 12:55 AM
Hello. Do you know what is a maximum DAC update rate for F446RE?
2016-09-09 2:07 AM
Hi,
Max DAC Update rate is 1Msps, this is mentioned in the (page 150).Regards2016-09-09 4:04 AM
For that 1Msps speed, the datasheet also notes ''Max frequency for a correct DAC_OUT change when small variation in the input code (from code i to i+1LSB)''
Previous versions of the datasheet used to quote the maximum DAC sample rate as 300ksps, but my observations of the (F407) DAC were that it is more a question of the maximum slew rate that the DAC can achieve; iirc it appeared to be around 1V/us.