cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX, cannot install FW package for STM32F4

mats23
Associate II
Posted on August 09, 2016 at 08:58

I am running CubeMX version 4.16.0, but I cannot update the firmware for STM32F4 to version 1.13.0.

When I do: Help->Install New Libraries and tick 1.13.0 and then ''Install Now'', the installer runs until it looks like the package has been downloaded, but then it throws ''These files have problem during download''.

I use Windows 10.

/M
4 REPLIES 4
macceb01
Associate II
Posted on August 09, 2016 at 09:45

I had the same problem but in this topic is solution [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Unable%20to%20Download%20STM32Cube%20packages&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=76]Unable to Download STM32Cube packages

Nesrine M_O
Lead II
Posted on August 09, 2016 at 10:39

Hi m_gustafsson,

I'll report this issue to our MX team for checking. Sorry for the inconvenience it may bring.

-Syrine-

mats23
Associate II
Posted on August 09, 2016 at 11:34

Thanks!

/M

mats23
Associate II
Posted on September 09, 2016 at 12:36

This is still an issue.

I see the same problem trying to upgrade CubeMX to 4.16.1.