2022-03-28 7:04 AM
Hi, I'm having the weirdest bug with this code. It's just 2 for loops expecting to count from 0 to 5 and 0 to 8.
When compiling with O3, i becomes very high and the execution gets stuck in the loops.
Running STM32 Cube IDE 1.9.0
STM32Cube FW_F4 V1.27.0
com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1
2022-03-28 7:08 AM
By the way, the loops use constants:
#define nbOutputRows 8
#define nbOutputGroups 5
2022-03-28 7:16 AM
It could be that i has been optimized out and the debugger doesn't monitor it correctly. I would imagine the access to outputs[] to cause a hard fault if i is absurdly high.
2022-03-28 7:36 AM
Enable at least minimal debug level (-g1) in the C/C++ Build Settings for the Release Config to get plausible values for local variables. It also makes sense to debug step-by-step, if possible at instruction level, to understand what's happening.
Make sure that the function calls have a side effect (like assigning to a volatile variable) and are not optimized out.
Comment out parts of your code ("bisecting") and observe changes.
Doubt that you caught a compiler bug.
hth
KnarfB
2022-03-28 7:39 AM
When I comment out line 110 it does say that "i" is optimized out and the infinite loop goes away.
2022-03-28 1:19 PM
Post sources of functions you use there, and disasm.
JW
2022-03-29 12:28 AM
The main difference between O2 and O3 seems to be the loop unrolling.
The function calls do have a side effect as it is setting a pin high or low in the loops:
if (gpioStatus)
gpioSet(COOUT); // Set
else
gpioReset(COOUT); // Reset
Changing the type of the table output[] to volatile fixed the issue in O3, the code no longer hangs and the loop counters work as expected (even though they struggle to show properly in the Expressions view).
I have attached the source file and the disasm compiled with O3.
2022-03-29 12:29 AM