F103 and F072 SPI communication
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-03 12:44 AM
I am trying to communicate with a device (a radio module which has inside STM32F103 MCU ) with my STM32f072B disco board using SPI
I can program the radio module almost as a standard STM32 MCU the only difference is that I don't have access to all pins.
Disco board is set as master, the RF module is a slave.
Both devices run at 16MHz; SPI prescaler is 256, 8bit data size, H polarity, 2edge phase, soft management of nss
I managed so far to output the clock signal but I don't have nothing on the MOSI line, allthough I'm sending data
I am not fully cleared about how the pins must be configured
The program for disco board:
#include 'stm32f0xx.h'
#define u8 uint8_t
#define u16 uint16_ttypedef uint32_t u32;typedef signed short s8;void spi1_config(void);
void delay(uint32_t t);#define NSS_Port GPIOA
#define NSS_Pin GPIO_Pin_4/* Private macro -------------------------------------------------------------*/
#define NSS_hi() NSS_Port->BSRR = NSS_Pin#define NSS_lo() NSS_Port->BRR = NSS_Pin/* Private variables ---------------------------------------------------------*//* Private function prototypes -----------------------------------------------*//* Private functions ---------------------------------------------------------*/
u8 t=0;extern u8 h;extern u8 y;/** * @brief Main program * @param None * @retval None */int main(void){ spi1_config();NSS_hi();
while(1) { delay(100); NSS_lo(); delay(150);SPI_SendData8(SPI1,0xab);
delay(200); NSS_hi(); }}void spi1_config(void)//master
{ GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; SPI_InitTypeDef SPI_InitStructure;/* Enable the SPI periph */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);/* Enable SCK, MOSI, MISO and NSS GPIO clocks */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA , ENABLE);GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;/* SPI SCK MOSI MISO pins configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7; GPIO_Init(GPIOA, &GPIO_InitStructure);/* SPI NSS pin configuration as GPIO Pin */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_Init(GPIOA, &GPIO_InitStructure);GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_0);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_0); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_0);/* SPI configuration -------------------------------------------------------*/
SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_InitStructure.SPI_Mode=SPI_Mode_Master;SPI_Init(SPI1, &SPI_InitStructure);
/* Initialize the FIFO threshold */
SPI_RxFIFOThresholdConfig(SPI1, SPI_RxFIFOThreshold_QF);SPI_NSSPulseModeCmd(SPI2,DISABLE);
SPI_SSOutputCmd(SPI2,DISABLE);/* Enable the Rx buffer not empty interrupt */
SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE);/* Configure the SPI interrupt priority */
NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = !ENABLE; NVIC_Init(&NVIC_InitStructure);/* Enable the SPI peripheral */
SPI_Cmd(SPI1, ENABLE);}void delay(uint32_t t)
{ for(;t!=0;t--) { asm('nop'); }}I can't see anything moving on the MOSI pin; only the SCK and NSS
Here is the code for the STM32F103 MCU
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
#include 'stm32f10x.h'
GPIO_InitTypeDef GPIO_InitStructure;
SPI_InitTypeDef SPI_InitStructure;NVIC_InitTypeDef NVIC_InitStructure;u16 t=0;
int main(void){ //GPIOA,GPIOB,GPIOC, USART1,SPI1 Periph clock enable RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_GPIOB|RCC_APB2Periph_GPIOC|RCC_APB2Periph_USART1|RCC_APB2Periph_SPI1, ENABLE); // USART2, I2C1, CAN1 Periph clock enable RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2|RCC_APB1Periph_I2C1|RCC_APB1Periph_CAN1|RCC_APB1Periph_TIM2,ENABLE);spi1_config();
while (1) { asm('nop'); }}
void spi1_config(void)//slave
{ //3. Configurare SPI1............................................................... //Configure SPI1 pins: SCK, MISO and MOSI ----------//Configure SCK, MOSI and NSS pins as floating inputs
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_7|GPIO_Pin_4; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure);// Configure MISO (slave out) pin as AF Push pull
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure);//SPI1 configuration ----------
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Slave; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure);//Disable SPI1 CRC calculation
SPI_CalculateCRC(SPI1, DISABLE);NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = !ENABLE; NVIC_Init(&NVIC_InitStructure);SPI_I2S_ITConfig(SPI1,SPI_I2S_IT_RXNE,ENABLE);
//Enable SPI1
SPI_Cmd(SPI1, ENABLE);}void delay(uint32_t t)
{for(; t != 0; t--){};
}Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-03 3:03 AM
I have discovered the issue....The 072Disco board have some solder bridges in order to conect the pins I used for SPI1 . On my board those solder bridges were unsoldered so the signals did not reach the pin header
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-03 1:13 AM
Hello
ionut.Fasoola
,ST is providing an example about the SPI usage. This will surely help you to correctly configure yourperipheral.
You can find the working example
inside the
library (v 1.7.0) under
this path:STM32Cube_FW_F1_V1.7.0\Projects\STM32F072B-Discovery\Examples\SPI.
May this help you.
If this solves your issue, please click on correct
:)
.Khouloud.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-03 3:01 AM
Thanks for sugestion. It seems i configured the pins correctly
Stil SPI does not output anything
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-03 3:03 AM
I have discovered the issue....The 072Disco board have some solder bridges in order to conect the pins I used for SPI1 . On my board those solder bridges were unsoldered so the signals did not reach the pin header
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-03 4:18 AM
Hi
ionut.Fasoola
,Glad that your issue is solved
And thanks for sharing the solution, this may be helpful for other users.Khouloud.