2010-08-23 12:51 AM
EXTI Lines
2011-05-17 05:03 AM
''I´m looking for in SMT32F103VE datasheet the pin description the EXTI lines but I didn´t searched them.''
Like several manufacturers these days, the ST Datasheet is largely just about physical parameters. Details about the actual operation are in a separate document. In the case of the STM32, the document you require is called the Reference Manual - see:2011-05-17 05:03 AM
It seems that I hadn´t explain enough well. I´ve RM0008,datasheet; insider guide, PM0056 docs, and I can´t search this data anywhere.
I´m trying to search where docs explains which pins are EXTI, what numbers and why?2011-05-17 05:03 AM
I´ve done it. There are 16 EXTI lines one per port Pin. So PA.0 is EXTI line 0 and so.