2019-02-01 03:51 AM
--- Problem solved! - as I can not delete the post, I edited this one
Solved! Go to Solution.
2019-02-01 03:55 AM
2019-02-01 03:55 AM
Ok, Problem solved!!!
Forgot to start the timer :\
2019-02-05 01:23 AM
Thanks for update, but it should be better to keep initial content of your post and mainly the symptoms of your problem. This should be helpful for other members that may face same issue.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-02-05 04:37 AM
Hello Amel,
ok, understood.
But I deleted the post because there was nothing special or wrong, except that the timer did not count the incoming pulses due to my missing "start the timer".
-Gaby-