Expected Speed of Flashing over USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-10 2:01 PM
Hello,
I am currently flashing an STM32F767 via the USART. I have no problems getting the device into DFU mode, initiating the flashing (Using STM32CubeProgrammer or stm32flash), etc., but the flashing time is between 6 and 7 minutes for the 1.3MB firmware image even at the maximum guaranteed baud of 115200. Having never utilized this flashing interface before, I'm not sure if this is expected.
I was wondering if anyone knew if there were strategies to speed up the flashing over USART and/or an expected size vs flash time one could expect in this configuration?
For reference, all my testing is being done on the NUCLEO-F767ZI via pins C11 and C10 using USART.
Thank you,
-Brian
Solved! Go to Solution.
- Labels:
-
STM32F7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-10 7:16 PM
The math suggests the minimum time would be 1.3MB / (115200*.8 bit/sec), or about 2 minutes. You can't possibly get better than that and due to the back and forth in the bootloader protocol, there is going to be substantial overhead.
6-7 minutes seems reasonable.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-10 3:43 PM
> I have no problems getting the device into DFU mode
Confused? DFU is not UART, it is the USB interface mode. STM32CubeProgrammer supports both modes, and more.
> at the maximum guaranteed baud of 115200
115200 is a common baud rate, but not very performant. Better use the USB interface (DFU or whatever available).
If you can flash using the ST-LINK on the Nucleo board, this may be the best option.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-10 5:27 PM
You could also stage code in RAM if you write to ST's protocol, and push something more efficient, self-pacing and robust. Like X or Y-Modem
Or commit a flash sector to a boot-loader supporting a standard protocol, from a terminal application sense, and that could support internal and external memorys.
ST has had a couple of IAP (In-Application Programming) examples
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-10 7:16 PM
The math suggests the minimum time would be 1.3MB / (115200*.8 bit/sec), or about 2 minutes. You can't possibly get better than that and due to the back and forth in the bootloader protocol, there is going to be substantial overhead.
6-7 minutes seems reasonable.