cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4: USART buffer overrun during Flash Erase operation

harisuvarna
Associate III

Hi ,

I am using STM32G4 to receive USART data from external interface and USART buffer overrun when USART interrupt conflicts with Flash Erase operation. 

As mentioned in STM32G4 Reference manual , in single bank mode, any read operation while writing/erasing flash 

stalls the bus until current flash operation is complete. To mitigate this performed following,

  • Moved ISR handler and subroutines invoked inside ISR to SRAM
  • Moved Interrupt Vector table to SRAM     

After all these changes , USART buffer still overruns when it conflicts with Flash erase operation

Request you to share your views.

Regards,

Hareesha

1 ACCEPTED SOLUTION

Accepted Solutions
harisuvarna
Associate III

Hi All,

Thanks for the response . Issue is resolved now.

  • Moved, Interrupt table , all  ISR handler and associated functions into CCM SRAM memory location.
  • Moved functions invoked after flash erase start to CCM SRAM memory location.

Refer application notes section 2.2 to execute ISR handler from CCM SRAM.

https://www.st.com/resource/en/application_note/an4296-use-stm32f3stm32g4-ccm-sram-with-iar-embedded-workbench-keil-mdkarm-stmicroelectronics-stm32cubeide-and-other-gnubased-toolchains-stmicroelectronics.pdf

 

Regards,

Hareesha

 

View solution in original post

7 REPLIES 7
Karl Yamashita
Principal

So there must be some command to have the STM32G4 to erase the flash. Do you not return and ack to let the external device start sending packets of data?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Hi ,

Thanks for the reply, Flash erase and write sequence works fine.  However  issue happens when Flash erase conflicts with USART data dequeuing. USART data reception is interrupt driven , data deque happens at UART ISR handler.

My understanding is Flash erase is interruptible. 

Regards,

Hareesha

Have you changed the interrupt priorities in the NVIC?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Why interrupt priority is required??. I don't use flash interrupt. I use only USART interrupt.

harisuvarna
Associate III

Also one more question, Can context switch happens when flash erase in progress?? CPU uses  AHB bus to perform Context switching.

Attach some code for the UART Callback and describe what you're doing to start the flash erase and the UART communication. And how much data are you receiving?

As @Methew mentioned, use the DMA in circular mode.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

harisuvarna
Associate III

Hi All,

Thanks for the response . Issue is resolved now.

  • Moved, Interrupt table , all  ISR handler and associated functions into CCM SRAM memory location.
  • Moved functions invoked after flash erase start to CCM SRAM memory location.

Refer application notes section 2.2 to execute ISR handler from CCM SRAM.

https://www.st.com/resource/en/application_note/an4296-use-stm32f3stm32g4-ccm-sram-with-iar-embedded-workbench-keil-mdkarm-stmicroelectronics-stm32cubeide-and-other-gnubased-toolchains-stmicroelectronics.pdf

 

Regards,

Hareesha