2025-02-12 11:37 PM
I am trying to create a Client that communicates via Ethernet on the PHY LAN8720 chip. The program has an error that does not run automatically when the board is powered on or the chip is reset. If I use debug, I have to press RUN several times to be able to access the config and main functions and then run normally. Can anyone help me with this error? Thank you very much!!!!