2018-09-10 2:00 AM
I use stm32h7 microcontroller and I want to make ethernet communication cubemx and keil .However I didn't find resources or examples.
2018-09-18 10:59 AM
Hi @Bilge ,
I recommend to refer to the example "LwIP_HTTP_Server_Netconn_RTOS" provided under the STM32H7 cube package. It's found under the path below:
STM32Cube\Repository\STM32Cube_FW_H7_V1.3.0\Projects\STM32H743ZI-Nucleo\Applications\LwIP
Also, refer to to the FAQ "Ethernet not working on STM32H7x3":
Link: https://community.st.com/s/article/FAQ-Ethernet-not-working-on-STM32H7x3
Khouloud.
2018-12-14 9:00 AM
Hello,
Is there a way to regenerate ico from the ethernet example ?
I find it really difficult to create functional ethernet if I just use stm32cubemx as a starting point.
So, I need to make the example our starting point for the project.
Thanks,
ran
2018-12-16 11:55 PM
Hi ,
You can make basic configuration on stm32cubemx because some settings come missing and failing to keil from cubemx .I have an application without rtos on my page ,You can look,but there was a packet loses and I din't find any solution .
2019-12-27 10:25 PM
hi @Bilge
I have the same problem, how did you solve your problem?
thanks.
2019-12-28 12:41 AM
Look at his profile - does it look like he has solved anything? No! Because CubeMX is made by ST's dumb code monkeys and is a swamp, in which you'll stuck and never make network and most of other parts working.
2019-12-30 12:28 AM