cancel
Showing results for 
Search instead for 
Did you mean: 

Error in initializing ST-LINK device. Reason: No device found on target.

MarktenKlooster
Associate II

 

Hi everyone,

 

I'm having trouble writing my program to my microcontroller, and I'm hoping someone can help.

When I tried to write my program in STM32CUBEIDE, I received the following message:

STMicroelectronics ST-LINK GDB server. Version 7.8.0 Copyright (c) 2024, STMicroelectronics. All rights reserved. Starting server with the following options: Persistent Mode : Disabled LogFile Name : C:\Users\markt\STM32CubeIDE\workspace_1.16.1\PCB_Test\Debug\st-link_gdbserver_log.txt Logging Level : 31 Listen Port Number : 61234 Status Refresh Delay : 15s Verbose Mode : Enabled SWD Debug : Enabled InitWhile : Enabled COM frequency = 4000 kHz Target connection mode: Under reset Target connection failed COM frequency = 1800 kHz Target connection mode: Under reset Target connection failed COM frequency = 950 kHz Target connection mode: Under reset Target connection failed COM frequency = 480 kHz Target connection mode: Under reset Target connection failed COM frequency = 240 kHz Target connection mode: Under reset Target connection failed COM frequency = 125 kHz Target connection mode: Under reset Target connection failed COM frequency = 100 kHz Target connection mode: Under reset Target connection failed COM frequency = 50 kHz Target connection mode: Under reset Target connection failed COM frequency = 25 kHz Target connection mode: Under reset Target connection failed COM frequency = 5 kHz Target connection mode: Under reset Target connection failed Target no device found Error in initializing ST-LINK device. Reason: No device found on target.
View more

 

Additionally, when I tried connecting using STM32CUBEProgrammer, I received this message:

19:58:54 : UR connection mode is defined with the HWrst reset mode 19:58:54 : ST-LINK SN : B55B5A1A000000006053F001 19:58:54 : ST-LINK FW : V2J45S7 19:58:54 : Board : -- 19:58:54 : Voltage : 3.30V 19:58:54 : Error: Unable to get core ID 19:58:54 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

 

 

I'm using an ST-Link V2 connected to a custom board via SWD. This is my first custom STM32 design, and here is the schematic:

MarktenKlooster_0-1740424090086.png

 

I have no idea where the issue might be. Any help would be greatly appreciated!

Thank you in advance for your assistance!

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
MarktenKlooster
Associate II

Hi everyone,

I have managed to fix the issue. There was probably something wrong with the ST-Link debugger. I have used another one, and now it's working!

 

Thank you all for your help!

View solution in original post

9 REPLIES 9
TDK
Super User

Schematic looks okay.

  • Verify part orientation. When text is oriented normally from left to right, pin 1 is on bottom left.
  • Verify VCAP voltages. Should be 1.2V.
  • Verify other power pins.
  • Verify SWD connections.

If you're using a knock-off programmer, note that it might just not work, especially with STM32CubeIDE. Use STM32CubeProgrammer until you can "connect" successfully--it is typically more robust.

If you feel a post has answered your question, please click "Accept as Solution".
AScha.3
Super User

Hi,

...and if your st-link is a stick (= clone), set connect : software reset (the "stick" has no reset output!)

AScha3_0-1740427147550.png

And try with CubeProgrammer first (more tolerant with clones...).

If you feel a post has answered your question, please click "Accept as Solution".

This is the st-link that I am using and how it is wired:

MarktenKlooster_0-1740429325306.jpeg

I'm unable to find the setting you mentioned.

Could you please provide more details?

 

in Cubeprogrammer:

AScha3_0-1740430723560.png

reset mode -> software

+

in IDE -> debug configuration -> same...

AScha3_1-1740430824423.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Hi,

Unfortunately, it did not work. I got the same result.

I also checked the part and all connections; however, they seem to be correct.

So show, what cubeProgrammer is telling ->

AScha3_0-1740490311167.png

 

If you feel a post has answered your question, please click "Accept as Solution".

MarktenKlooster_0-1740490523261.png

MarktenKlooster
Associate II

Hi everyone,

I have managed to fix the issue. There was probably something wrong with the ST-Link debugger. I have used another one, and now it's working!

 

Thank you all for your help!


@MarktenKlooster wrote:

There was probably something wrong with the ST-Link 


It was not a genuine ST-Link:

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/tac-p/703663/highlight/true#M965 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.