2019-11-21 3:41 AM
Hi,
I'm trying to transmit some data using FD-CAN but HAL_FDCAN_Start() function returns error code 38. I have taken reference from STM32H743-EVAL kit example.I have configured same as mentioned there. But still i couldn't figure out the issue behind it.
Thanks,
Vimal
2019-11-21 9:25 PM
Hi,
that issue is solved, Tx fifo/queue was not allocated into RAM area, Now my tx fifo is not getting cleared after transmission of message,
/* Retrieve the Tx FIFO PutIndex */
PutIndex = ((hfdcan->Instance->TXFQS & FDCAN_TXFQS_TFQPI) >> FDCAN_TXFQS_TFQPI_Pos);
/* Add the message to the Tx FIFO/Queue */
FDCAN_CopyMessageToRAM(hfdcan, pTxHeader, pTxData, PutIndex);
/* Activate the corresponding transmission request */
hfdcan->Instance->TXBAR = ((uint32_t)1 << PutIndex);
/* Store the Latest Tx FIFO/Queue Request Buffer Index */
hfdcan->LatestTxFifoQRequest = ((uint32_t)1 << PutIndex);
also i'm not seeing any data after transmission, what could go wrong for unsuccessful transmission?
how do i proceed further, someone please help me!
Thanks,
Vimal
2019-11-22 1:48 AM
issue is solved..there was a placement issue in crystal oscillator
2022-01-05 10:05 PM
can we run FDCAN without using external oscillator
2023-12-11 11:09 PM
How did you fix the error?