cancel
Showing results for 
Search instead for 
Did you mean: 

Error: Cannot Find the interface for Communication Interface Class

Milad_
Associate

Hello everyone,

I'm working on controlling my serial modem using the STM32 Nucleo G0B1 board. I've configured the Nucleo as a USB host, and my modem is a CDC-ACM device. I've set up the USB settings in CubeIDE and connected the modem to the Nucleo using a USB cable. I've attached the output of ST-Link for debugging purposes. Everything seems to be working fine until the "HOST CLASS CHECK" stage, where I encountered an error.

Could you please assist me in establishing communication with my modem and resolving this issue?

Thank you for your help.

err-stm32.jpg

1 REPLY 1
FBL
ST Employee

Hi @Milad_ 

Do you still have issue while communicating with your modem?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.