Ensuring that goto from one function to another function always works properly?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 2:09 AM
I am working with the STM32F446 microcontroller and compiling with Eclipse/GCC.
Short version: I have two functions, main1(int argc, char* argv[]) and main2(int argc, char* argv[]) and I want to be able to goto back and forth between the two many times. What do I need to do to ensure that this will always work properly? In particular, I'm concerned about the stack and the Core General Purpose Registers R0...R12. Will these be "confused" if they all of a sudden find themselves executing inside a different function or will it be just fine since I always goto the BEGINNING of the respective functions?
Long version: I need to make my own USB-bootloader (no, the built-in bootloader doesn't fit my needs) and I have two Eclipse projects, bootloader project at sectors 0-3 and application project at sectors 4-7. I need to somehow be able to switch between bootloader mode and application mode (and vice versa) without dropping the USB-connection (hence, I can't reset the microcontroller). If I switch between the two projects using function CALLS, then I'm afraid I will run of out stack in case someone switches back and forth many times, that's why I want to switch between the two using goto instead.
- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 3:22 AM
Is it possible to readjust the stack pointer (copying the stack in the starting position also) to start always at the beginning of the stack?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 4:54 AM
How about a "controlling" main that alternately calls main1 and main2?
To switch between, all you need do is return from your current mainx
How strongly do you need to not drop the USB connection? My guess is that firmware upgrades don't happen all that often so they're allowed to be sufficiently slow to re-establish USB.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 5:10 AM
Not sure if it fits your use case: setjmp + longjmp came to my mind.
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 5:22 AM
You tell me. Is that all that's necessary to do?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 5:25 AM
Interesting idea, I think that should work. If the USB-connection is dropped, the re-connects are flaky and computer dependent (look at the Device Manager when you add/remove a USB-device, sometimes the tree gets updated 3-4 times) making the product appear to be of low quality.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 5:26 AM
Wow, that is way above my level, I have no idea what that means.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 5:39 AM
Alternatively, jumping from a bootloader to the main application won't reset the USB. It will be in the same state as when the jump happened. You will need to ensure interrupts stay enabled through the transition and that the vector table entry for USB is valid, but these are solvable problems. Set flags to indicate where the code is at and act accordingly in the interrupt.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 5:52 AM
Yes, I will specify SCB->VTOR first thing in main, in both bootloader and application. I was planning to hardcode a shared location in RAM for static and global variables. However, you brought up a good point about code in flash, I'm not sure how to solve that. I want the bootloader to be able to work even if the application area (sectors 4-7) is erased and I want to be able to run the application without the bootloader (common case when debugging from Eclipse). Could you please elaborate on how to use flags to indicate where the code is?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-16 6:00 AM
Code in flash stays in flash after the jump. The variables may not, but the code is there. You just need to ensure the variables that it does access are valid. Hence, the shared flag.