2018-08-14 8:02 AM
How can I enable the parity check in the SRAM 2 of the STM32L4?
Is there a HAL function?
2018-08-14 8:32 AM
You have to configure a bit in the Options Bytes, try looking at related examples for reading/writing those and extend to your requirements
STM32Cube_FW_L4_V1.12.0\Projects\STM32L476G-EVAL\Applications\IAP\IAP_Main\Src\flash_if.c
STM32Cube_FW_L4_V1.12.0\Projects\32L476GDISCOVERY\Examples\FLASH\FLASH_DualBoot\Src
STM32Cube_FW_L4_V1.12.0\Projects\32L476GDISCOVERY\Examples\FLASH\FLASH_WriteProtection\Src
STM32Cube_FW_L4_V1.12.0\Drivers\STM32L4xx_HAL_Driver\Src\stm32l4xx_hal_flash_ex.c
/**
* @brief Program the FLASH User Option Byte.
*
* @note To configure the user option bytes, the option lock bit OPTLOCK must
* be cleared with the call of the HAL_FLASH_OB_Unlock() function.
* @note To validate the user option bytes, the option bytes must be reloaded
* through the call of the HAL_FLASH_OB_Launch() function.
*
* @param UserType: The FLASH User Option Bytes to be modified
* @param UserConfig: The FLASH User Option Bytes values:
* BOR_LEV(Bit8-10), nRST_STOP(Bit12), nRST_STDBY(Bit13), IWDG_SW(Bit16),
* IWDG_STOP(Bit17), IWDG_STDBY(Bit18), WWDG_SW(Bit19), BFB2(Bit20),
* DUALBANK(Bit21), nBOOT1(Bit23), SRAM2_PE(Bit24) and SRAM2_RST(Bit25).
*
* @retval HAL status
*/
static HAL_StatusTypeDef FLASH_OB_UserConfig(uint32_t UserType, uint32_t UserConfig)
{
..
if((UserType & OB_USER_SRAM2_PE) != 0U)
{
/* SRAM2_PE option byte should be modified */
assert_param(IS_OB_USER_SRAM2_PARITY(UserConfig & FLASH_OPTR_SRAM2_PE));
/* Set value and mask for SRAM2_PE option byte */
optr_reg_val |= (UserConfig & FLASH_OPTR_SRAM2_PE);
optr_reg_mask |= FLASH_OPTR_SRAM2_PE;
}
2018-08-15 11:19 PM
FLASH_OB_UserConfig() is a static function. I use HAL_FLASHEx_OBProgram() which calls FLASH_OB_UserConfig():
HAL_FLASHEx_OBGetConfig(&optionBytesInit);
optionBytesInit.USERType |= OB_USER_SRAM2_PE;
optionBytesInit.USERConfig &= ~FLASH_OPTR_SRAM2_PE_Msk;
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBProgram(&optionBytesInit);
HAL_FLASH_OB_Lock();
HAL_FLASH_OB_Launch();
But HAL_FLASH_OB_Unlock() generates a hard fault.
2018-08-16 1:02 AM
Do you have some of the lock or other options set through device programming?
JW
2018-08-16 5:30 AM
I don't set anything actively during programming, but we use IAR (V8.20) and HAL (V1.8.3).
The value of the option register (FLASH->OPTR) is 0xFFEFF8AA.
2018-11-02 7:38 AM
Do someone from ST could check if the SRAM2 parity enable bit can be reset to 0 (0 = parity check enabled!) in the STM32L4A6ZG?
The code in not working:
FLASH_OBProgramInitTypeDef optionBytesInit = {0U};
HAL_FLASHEx_OBGetConfig(&optionBytesInit);
optionBytesInit.USERType |= OB_USER_SRAM2_PE;
optionBytesInit.USERConfig &= ~FLASH_OPTR_SRAM2_PE;
HAL_FLASH_OB_Unlock();
HAL_FLASH_Unlock();
HAL_FLASHEx_OBProgram(&optionBytesInit);
if (HAL_FLASH_OB_Launch() != HAL_OK)
{
while(1);
}
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
The SRAM2_PE is always 1 (instead of 0).
And a bus fault arise afterwards.
2018-11-02 8:09 AM
>>Do someone from ST could check if the SRAM2 parity enable bit...
This is predominantly a user forum, you should work with the ST FAE supporting your account, or those at your distributor. Or file an Online Support request.