2023-05-04 12:27 AM - last edited on 2023-09-01 09:21 AM by Amel NASRI
Hi ST community,
First question for me here.... It is about an emulated eeprom issue
I try to save dta to an emulated eeprom.
Parameter are : starting dress : 0x800D00
page size 0x800
number of variable to be saved 37
guard page number =2
cycle life =1
I do manage to save and read from eeprom however, after a while (let's say between 500 and 1000 saving operations, the eeprom comes into the loop below and don't mnage to get out...
Would somebody knows why ? I assume my parameters are wrong but I can't figure it out ...
Thanks ,
Tjhe loop that blocks ...
pageadress takes the value 28 27 26 and then back to 28.
while ((pagestate == STATE_PAGE_ACTIVE) || (pagestate == STATE_PAGE_VALID) || (pagestate == STATE_PAGE_ERASING))
{
/* Set counter index to last element position in the page */
counter = PAGE_SIZE - EE_ELEMENT_SIZE;
/* Check each page address starting from end */
while (counter >= PAGE_HEADER_SIZE)
{
/* Get the current location content to be compared with virtual address */
addressvalue = (*(__IO EE_ELEMENT_TYPE*)(pageaddress + counter));
if (addressvalue != EE_PAGESTAT_ERASED)
{
/* Compare the read address with the virtual address */
if (EE_VIRTUALADDRESS_VALUE(addressvalue) == VirtAddress)
{
/* Calculate crc of variable data and virtual address */
crc = CalculateCrc(EE_DATA_VALUE(addressvalue), EE_VIRTUALADDRESS_VALUE(addressvalue));
/* if crc verification pass, data is correct and is returned.
if crc verification fails, data is corrupted and has to be skip */
if (crc == EE_CRC_VALUE(addressvalue))
{
/* Get content of variable value */
*pData = EE_DATA_VALUE(addressvalue);
return EE_OK;
}
}
}
/* Next address location */
counter -= EE_ELEMENT_SIZE;
}
/* Decrement page index circularly, among pages allocated to eeprom emulation */
page = PREVIOUS_PAGE(page);
pageaddress = PAGE_ADDRESS(page);
pagestate = GetPageState(pageaddress);
}
Solved! Go to Solution.
2023-05-17 02:22 AM
cleanup seems to solve the problem once I update
ee_status=
to
ee_status|=
thanks
2023-05-04 12:40 AM
Hello,
Could you please tell me on which device you are working please and show your applicative code?
2023-05-04 12:51 AM
hi, Thanks for your answer : the uC is an stm32G071
typical application code looks like this :
EE_WriteVariable16bits((int *)cAddr_cusaR0Mes , usa_Temp[0]);
EE_WriteVariable16bits((int *)cAddr_cusaR0E0 , usa_Temp[1]);
EE_WriteVariable16bits((int *)cAddr_cusaR0EM , usa_Temp[2]);
EE_WriteVariable16bits((int *)cAddr_cusaR0CapTequ , usa_Temp[3]);
EE_WriteVariable16bits((int *)cAddr_cusaR0CapConso , usa_Temp[4]);
EE_WriteVariable16bits((int *)cAddr_cusaR0Ibat , usa_Temp[5]);
EE_WriteVariable16bits((int *)cAddr_cusaR0Ubat , usa_Temp[6]);
EE_WriteVariable16bits((int *)cAddr_cusaR0State , usa_Temp[7]);
EE_WriteVariable16bits((int *)cAddr_cusaCodeBatModeAlrm, usa_Temp[8]);
2023-05-04 01:45 AM
Perhaps you could make a trial with a starting address @ 0x0801 0000 ?
Are you sure your flash is free@ 0x0800D000?
2023-05-04 02:10 AM
yes it is free down to 0x0800C000
2023-05-04 02:24 AM
Ok if you can try to change the starting address @ 0x0801 0000 to check it's not the problem..
2023-05-04 03:14 AM
I will and I let you know
2023-05-09 07:51 AM
Hi Chloe,
There isn't actually enough space between 0x8010 0000 and the end of the flash to be able to load all pages ...
(indeed) I got error message while loading with this parameter :
"Break at address "0xfffffffe" with no debug information available, or outside of program code."
Edgar
2023-05-09 07:56 AM
Hello Edgar,
Yes I wrote @ 0x0801 0000 not 0x8010 000 :-)
2023-05-09 08:00 AM
Sorry, I did write it wrong. Indeed, I used 0x0801 0000 and got this error not 0x8010 0000
//#define START_PAGE_ADDRESS 0x08010000U /*!< Start address of the 1st page in flash, for EEPROM emulation */
#define START_PAGE_ADDRESS 0x0800C800U /*!< Start address of the 1st page in flash, for EEPROM emulation */
#define CYCLES_NUMBER 1U /*!< Number of 10Kcycles requested, minimum 1 for 10Kcycles (default),
for instance 10 to reach 100Kcycles. This factor will increase
pages number */
#define GUARD_PAGES_NUMBER 2U /*!< Number of guard pages avoiding frequent transfers (must be multiple of 2): 0,2,4.. */