cancel
Showing results for 
Search instead for 
Did you mean: 

Editing variables during debugging...

magas09
Associate II
Posted on April 08, 2015 at 20:26

Hi!

I am using the stm32f429zi board and compiling it on CooCox 1.7.7 and I am a beginner in embedded programming...

During the debugging of my project, the debugger cannot see changes in variables and shows them as zeros (this variables are also not-editable)... Some variables are editable (which has lower addresses) but above some address, which I don't know, they cannot be changed...

Application works correct with this variables because they are displayed on the LCD... I don't know why the debugger can't see values of some variables...

Is it possible to fix it...? What can I do...?

Thanks a lot for any hints,

best regards,

Marcin

#debugger #coocox
1 REPLY 1
Posted on April 08, 2015 at 20:32

CooCox has their own support forum, seek support there.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..