2018-01-12 1:21 PM
Are older versions of
STM32CubeF2 available? I am trying to find some files that were not included in a project I am working on. From looking at some of the files we do have, I see:
* @version V1.1.2
* @date 11-December-2015Several files I checked match that, so I think I am looking for V1.1.2.
Any pointers where to look? My searches didn't lead me to any answers.
Thanks!
Solved! Go to Solution.
2018-01-12 3:20 PM
Just tried out of curiosity - one day I may need the same for myself;)
2018-01-12 3:22 PM
Yes, right. I believe that jive is self-destroying beast;) Just because of built-in complexity.
2018-01-12 5:11 PM
1.1.1 was a delta from 1.1.0 (ie unpacks into the same directory tree adding or overwriting some files)
https://drive.google.com/open?id=0B7OY5pub_GfIUFJuZGltcUdRR28
2018-01-15 10:49 AM
I had some projects using later versions (from just a few months ago), so I decided to update them while I was at it. It appears the version numbers have been removed from the header comments in the files (@version and @date). For tracking purposes, I'm going to start checking in the Release Notes file(s) so we at least know what version we are using.
Is there a different way to tell versions of the current HAL code?
2018-01-15 12:32 PM
Usually the code is placed in the repository with a directory name reflecting the primary release. The Z in vX.Y.Z is usually provided as a small differential patch.
CubeMX can download different versions of the code. You should perhaps add your own notes/comments in USER sections of your project code reflecting when it was built and the versions of libraries and tools used. Here we also archive libraries and documentation.
2018-01-15 2:12 PM
We are working with legacy repositories and projects, so our ability to change things is limited.
However, as soon as we make a new, clean project, there will be changes. Many changes.
2018-02-02 12:51 PM
Looking at a recent package, en.stm32cubef2 (v1.6.0), I see that the HAL inside is labeled as 1.2.1:
* @file stm32f2xx_hal.c
* @author MCD Application Team * @version V1.2.1 * @date 14-April-2017How do I find which version of CubeF2 contains HAL 1.1.2?
We are having issues with UART code, as it turns out, and release notes show some changes happened with 1.1.3. We are trying to get an unmodified 1.1.2 to make sure it wasn't some customization we made years ago.
2018-02-05 9:59 AM
Thanks for this. My coworker was able to figure out which package we needed that contained the old 2015 version we were using.
2018-03-12 7:39 AM
Beyond installing the Cube software and doing the config hacks, mentioned above, does anyone know how I can get F@ HAL version:
V1.1.3 / 29-June-2016
2018-03-12 9:25 AM
I tried this today and I did not have any similar line to:
ProjectManager.FirmwarePackage=
I saw it download 1.7.x for the sample project I created, but I did not see any updates to the .ioc file.
What version of the CubeMX software were you using?