2017-05-29 8:16 AM
Hello everybody.
I want to sample A0 (ADC1) and A1 (ADC2) in the dual regular simultaneous mode (Trigger Timer 2).
So I have created a Project with cubemx (Nucleo-F446RE) and HAL-Libary.
The Problem is that the conversion starts only one time. So if I change the potentiometer the value from the ISR-Variable is not update.
Maybe someone have got more experiance with this ADC-mode an can help me!
Thanks,
Flo