DSP Sampling Rate, FFT Size, and Buffer Size
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-07-25 12:46 PM
Hi,
Can someone please throw some ideas on what might be the problem with what I am seeing / doing. Here are the relevant details. 1 - Using an STM32F407 processor (Discovery PCB), clock at 168Mhz2 - Using ADC to sample low frequency signals (< 50Hz) from sensors
3 - Have timer interrupt set such that setting timer period to frequency will interrupt at that rate and add a sample from ADC to buffer. Using timestamps, I have confirmed that the interrupt is operating correctly
4 - I have a filter coefficient (400 taps) at Fs = 512Hz, and 1024Hz. The reason I'm using power of 2 values for sampling is so that when I divide the sampling rate into the FFT size, I should get 0.5Hz resolution. (according to resolution = Fs / Fn)
In the header, I have three &sharpdefines that control the interrupt operation:
&sharpdefine SAMPLE_FREQ
&sharpdefine BUFFER_SIZE
&sharpdefine FFT_SIZE
In the interrupt handler:
if(sampleCount == BUFFER_SIZE)
{
inputBufPtr = &ADC_Values[0];
outputBufPtr = &outputBuffer[0];
arm_fir_instance_f32 S;
arm_fir_init_f32(&S, FILTER_TAP_NUM, (float32_t *)&filter_taps[0], &firStateF32[0], BLOCK_SIZE);
for(uint16_t i = 0; i < NUM_BLOCKS; i++)
{
arm_fir_f32(&S, inputBufPtr + (i * BLOCK_SIZE), outputBufPtr + (i * BLOCK_SIZE), BLOCK_SIZE);
}
if( FFT_SIZE == 512 )
arm_cfft_f32(&arm_cfft_sR_f32_len512, outputBuffer, ifftFlag, doBitReverse);
if( FFT_SIZE == 1024 )
arm_cfft_f32(&arm_cfft_sR_f32_len1024, outputBuffer, ifftFlag, doBitReverse);
else if( FFT_SIZE == 2048 )
arm_cfft_f32(&arm_cfft_sR_f32_len2048, outputBuffer, ifftFlag, doBitReverse);
/* Calculate the magnitude at each bin */
arm_cmplx_mag_f32(outputBuffer, cfftBuffer, FFT_SIZE);
//zero the DC component
cfftBuffer[0] = 0;
//do stuff here...look for bins of interest....
} //end: if (samplecount...
So this is where my questions are:
With the defines set to these values:
&sharpdefine SAMPLE_FREQ 512
&sharpdefine BUFFER_SIZE 2048
&sharpdefine FFT_SIZE 1024
And using the Dolph-Cheby filter coefficients for Fs = 512, with a 22Hz sensor signal into the ADC, here are the bin values from 1 to 25:
Power at 1 = 201.5
Power at 2 = 203.8
Power at 3 = 183.8
Power at 4 = 215.4
Power at 5 = 137.4
Power at 6 = 107.9
Power at 7 = 112.4
Power at 8 = 125.5
Power at 9 = 81.0
Power at 10 = 128.6
Power at 11 = 190.1
Power at 12 = 60.5
Power at 13 = 53.6
Power at 14 = 103.9
Power at 15 = 76.4
Power at 16 = 84.4
Power at 17 = 29.6
Power at 18 = 61.4
Power at 19 = 48.9
Power at 20 = 18.0
Power at 21 = 40.9
Power at 22 = 47.6
Power at 23 = 524.6
Power at 24 = 123.5
Power at 25 = 55.9
Power at 58 = 43.9
Power at 59 = 96.4
The sensor is signalling at precisely 22Hz, but the highest bin level is at 23, one higher than it should be.
Now, if I set the defines to these values:
&sharpdefine SAMPLE_FREQ 1024
&sharpdefine BUFFER_SIZE 2048
&sharpdefine FFT_SIZE 1024
And use the Dolph-Cheby filter coefficients for Fs = 1024, here are the new bin values (shown from 20 to 50):
Power at 21 = 197.2
Power at 22 = 64.0
Power at 23 = 81.5
Power at 24 = 70.8
Power at 25 = 72.8
Power at 26 = 49.3
Power at 27 = 31.5
Power at 28 = 37.9
Power at 29 = 7.5
Power at 30 = 18.7
Power at 31 = 20.3
Power at 32 = 30.4
Power at 33 = 17.6
Power at 34 = 27.1
Power at 35 = 67.4
Power at 36 = 28.9
Power at 37 = 12.6
Power at 38 = 29.6
Power at 39 = 14.5
Power at 40 = 52.4
Power at 41 = 46.9
Power at 42 = 44.1
Power at 43 = 21.2
Power at 44 = 28.1
Power at 45 = 89.8
Power at 46 = 311.5
Power at 47 = 236.7
Power at 48 = 83.2
Power at 49 = 54.1
Power at 50 = 35.7
The high bin has now moved to 46. Dividing by 2 and subtracting 1 it is 22, which again is correct.
Can someone provide some insight as to why this is? Any comments or suggestions would be appreciated.
Thanks!
#dsp #adc #sampling-rate #timer-i