cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32F030 series have single-cycle multiplication?

wqluck
Associate
Posted on August 31, 2014 at 15:33

I am not sure if the MCU STM32F030 has single-cycle multiplication,which is based on the ARM Cortex-M0 core? Anybody knows that please help me.I want to use this MCU for motor control,is that suitable?Thanks.

Best Wishes!

#rtfm
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 31, 2014 at 20:01

http://www.st.com/web/en/resource/technical/document/programming_manual/DM00051352.pdf

 

''The Cortex-M0 processor is built on a highly area and power optimized 32-bit processor

 

core, with a 3-stage pipeline von Neumann architecture. The processor delivers exceptional energy efficiency through a small but powerful instruction set and extensively optimized design, providing high-end processing hardware including a single-cycle multiplier.''
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
wqluck
Associate
Posted on September 01, 2014 at 03:58

Thank you very much!