Does the signal SAI2_FS_A not trigger when SAI 2 is in synchronous slave mode?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-06 1:19 PM
Hi there,
I'm using the SAI2_FS_A signal to trigger a capture event on TIM2 (Through a series of weird internal routing). It all works nicely when SAI2 is an asynchronous master, however in my application it needs to be a synchronous slave to SAI1. I understand that there is no SAI2 FS signal output on a pin when in slave mode, but is the internal signal also disabled?
It's not working for me and I really hope there's an option or work around!
Many thanks,
Matt
Labels:
- Labels:
-
SAI
-
STM32H7 series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0