2018-08-16 12:41 AM
The Reference manual states that the FDCAN supports CAN FD according to specification 1.0, but also states it is ISO 11898-1:2015 conformant.
Also: There is a bit in one of the control registers that suggests the FDCAN can support both versions. Is that actually true?
Thanks
2018-08-16 02:43 AM
Hello Frank,
Correct! As indicated in the reference manual, both modules (FDCAN1 and FDCAN2) are compliant with ISO 11898-1: 2015 (CAN protocol specification version 2.0 part A, B) and CAN FD protocol specification version 1.0.
Khouloud.