2024-03-25 10:54 AM - edited 2024-03-25 3:05 PM
Hi,
I'm trying to check I3C protocol with NUCLEO-H503RB and IKS01A1.
I just followed below link for I3C.
https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3C
And I can see that the master transmit the data but there is no ACK from the slave.(I've attached the scope shot).
I was trying to buy IKS01A3, but it was out of stock, so I just bought IKS01A1. Because it seems same IC. Is it okay?
I've also tried below example from the github, but result is same.
https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H503RB/Examples/I3C
Please help me to find a way to check I3C.
Solved! Go to Solution.
2024-03-29 9:51 AM
Thank you for reply.
I found reason because I set the clock 12500 Khz which is maximum.
After I change it to 3000Khz which is recommended by that link. it works well.
Thank you anyway.
2024-03-29 4:49 AM
Hello @LukeJang522 ,
Have you checked the below examples, which may help you?
These examples use X-NUCLEO-IKS4A1A and X-NUCLEO-IKS01A3.
For you information, the X-NUCLEO-IKS01A1 is Not Recommended for New Design as shown in this link.
So, you can use this link to buy X-NUCLEO-IKS01A3.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-29 9:51 AM
Thank you for reply.
I found reason because I set the clock 12500 Khz which is maximum.
After I change it to 3000Khz which is recommended by that link. it works well.
Thank you anyway.