cancel
Showing results for 
Search instead for 
Did you mean: 

Do I need to install external crystal for STM32

OElso.1
Associate

I just got an STM32 Nucleo 64 - F411RE.

The board has a crystal installed on the debugger, and a crystal oscillator on the board.

Do I need to install an external crystal in the provided space X3? and how can I do so?

It's my first time using STM32 I don't really know what to do.

I will be using the board with FREE RTOS to drive motors for a robotic arm.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

No, you don't need to install a crystal. The 8MHz clock source coming from the ST-Link chip is driven by a crystal and is very accurate. Even if the crystal wasn't there, you could use the internal HSI clock source with decent accuracy.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

No, you don't need to install a crystal. The 8MHz clock source coming from the ST-Link chip is driven by a crystal and is very accurate. Even if the crystal wasn't there, you could use the internal HSI clock source with decent accuracy.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks a lot for your help