cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L562: frequency error when outputting LSE via MCO (crystal mode); bypass OK

Jerry_Cao
Associate II

Hi everyone,

I’m using an STM32L562 MCU and outputting LSE (32.768 kHz) to MCO for measurement.
In LSE crystal mode, I see a large frequency deviation on the oscilloscope (much larger than expected ppm-level error).

To rule out the crystal itself, I checked the 32.768 kHz crystal and it seems OK.

Then I tried LSE bypass mode (feeding an external 32.768 kHz clock into the LSE pins). In this case, the MCO output frequency error becomes very small, and the waveform/frequency looks correct.

So I suspect there might be an issue with the LSE oscillator circuit (load caps, PCB layout, drive strength, leakage, etc.) when running in crystal mode.

Questions:

  1. Has anyone experienced large LSE frequency error in crystal mode on STM32L562 / STM32L5 series?

  2. Any common root causes (wrong load capacitors, stray capacitance, drive level, board leakage, etc.)?

  3. Any recommended debugging steps or configuration tips (e.g., LSE drive settings, oscillator startup behavior, measurement method, etc.)?

Thanks in advance!

 

Here is my test code :

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
  Error_Handler();
 }

 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_HIGH);

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI
 |RCC_OSCILLATORTYPE_LSE
 |RCC_OSCILLATORTYPE_LSI;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_11; // 48 MHz on L5
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV1;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;

 /* We no longer need PLL as system clock */
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_OFF;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
  Error_Handler();
 }

 HAL_RCCEx_EnableMSIPLLMode();

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK |
 RCC_CLOCKTYPE_SYSCLK|
 RCC_CLOCKTYPE_PCLK1 |
 RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; // HCLK = 48 MHz
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; // PCLK1 = 48 MHz
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; // PCLK2 = 48 MHz
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
  Error_Handler();
 }

 // __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI);

 HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_LSE, RCC_MCODIV_1);
 //HAL_RCCEx_EnableLSCO(RCC_LSCOSOURCE_LSE);
}

Edited to apply source code formatting - please see How to insert source code for future reference.

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @Jerry_Cao and welcome to the ST community,

Did you refer to the application note: AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs" / section "3.7 Crystal pullability" ? It could be linked to the CL capacitance.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Andrew Neil
Super User

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

Also: How to insert source code

 

In particular, please give details of your hardware setup (schematics, etc), tools, etc.

 

It would be better to use your scope's image download facility - then you won't get all the blur, reflections, unwanted background, etc of a photograph.

 


@Jerry_Cao wrote:

Here is my test code


Is that from CubeMX, or manually written?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Employee

Hello @Jerry_Cao and welcome to the ST community,

Did you refer to the application note: AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs" / section "3.7 Crystal pullability" ? It could be linked to the CL capacitance.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Almost the same discussion here.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
TDK
Super User

> To rule out the crystal itself, I checked the 32.768 kHz crystal and it seems OK.

How exactly did you do this? Just look at it and say "yep, that's a crystal"?

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for your support. The reference manual is very helpful. But i have another question. I tried probing OSC32_OUT directly with an oscilloscope probe, but it is very small. So i want to know:

Is there any typical/expected voltage amplitude range on OSC32_OUT (e.g., mVpp / Vpp) when LSE crystal mode is running normally on STM32L562 / STM32L5?

Another question = new thread.

So the question here did we answer your original question : "frequency error when outputting LSE via MCO (crystal mode)" ?

If yes please mark Accept as Solution the post that answered your question or guided you to the solution and open a new thread for a new question.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

ok, i will start a new thread.


New thread: question about OSC32_OUT amplitude (STM32L562 LSE crystal mode).