cancel
Showing results for 
Search instead for 
Did you mean: 

Do ADCs have independent input channels in dual mode?

RGris
Associate II

I want to use ADC1 and ADC2 in dual mode simultaneous. In reference manual on p.360 there is a note that states that i can't convert tha same channel on both ADCs simultaneously ("no overlapping sampling times for the two ADCs when converting the same channel"). In my case on both ADCs channels 1 and 3 are used, but the channels of ADC1 and ADC2 are (as usual) mapped to different pins. Why can't I convert simultaneously ADC1_CH1 and ADC2_CH2 if these channels are phisically different and each ADC has it's own sampling circuit? Do ADCs have independent input channels in dual mode or share some common set of channels?

5 REPLIES 5
Olivier GALLIEN
ST Employee

Hi @RGris​ 

Can you please specify which STM32 you are using ?

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RGris
Associate II

STM32F303CC

RM

Thanks, remove topic "STM32 MPUs" then and add STM32F3.

This should help to reach relevant people for support.

BR

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Olivier as far as I concern this quastion already has topic "STM32F3"

Sould I remove "STM32 MCUs" (not MPU)?

No it's ok like this.

STM32 MCUs is parent topic containing STM32F3 but this is to get wider audience for your ticket.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.