2013-04-15 6:04 AM
Hello,
I'm trying to configure DMA2 stream 0 to do a transfer from external SRAM on the FSMC to a SSD1963 Display controller also on the FSMC. This is my code can't seem to get it working, I assume this is possible?/* Enable DMA clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); DMA_DeInit(DMA2_Stream0);while (DMA_GetCmdStatus(DMA2_Stream0) != DISABLE)
{ } /* Configure DMA Stream */ LCD_DMA_InitStructure.DMA_Channel = DMA_Channel_0; LCD_DMA_InitStructure.DMA_PeripheralBaseAddr = 0x68000000; LCD_DMA_InitStructure.DMA_Memory0BaseAddr = 0x6C000002; LCD_DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToMemory; LCD_DMA_InitStructure.DMA_BufferSize = 0x320; LCD_DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Enable; LCD_DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; LCD_DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; LCD_DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; LCD_DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; LCD_DMA_InitStructure.DMA_Priority = DMA_Priority_High; LCD_DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; LCD_DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; LCD_DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_INC4; LCD_DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_INC4; DMA_Init(DMA2_Stream0, &LCD_DMA_InitStructure); DMA_ClearFlag(DMA2_Stream0, DMA_IT_TC); /* Enable DMA Stream Transfer Complete interrupt */ DMA_ITConfig(DMA2_Stream0, DMA_IT_TC, ENABLE); // DMA Stream enable DMA_Cmd(DMA2_Stream0, ENABLE); #dma-stm32f4-fsmc-sram2013-04-15 9:39 PM
''Manual'' transfers do work?
Why the ''odd'' address (not multiple of 4)? JW2013-04-16 12:28 AM
JW,
Manual transfers are working fine, I just need to take some load off the CPU. The address also works fine on a manual write, the SSD1963 registers are toggled by A0 on a 16 bit bus. Thanks2013-04-16 2:13 AM
OK, and DMA with no bursts would work?
I am not sure your setup does not violate the rules for bursts, e.g. the 1kB address boundary rule. JW2013-04-17 1:00 AM
JW,
I've tried it with single burst, this didn't work. The stream never seems to get enabled. Thanks2013-04-19 6:58 AM
JW,
I've got it working now! I wasn't always calling DMA_DeInit(DMA2_Stream0); before I started writing out another line to the LCD via the DMA. works OK in single burst with FIFO. Thanks2013-04-19 7:54 AM
> I wasn't always calling DMA_DeInit(DMA2_Stream0);
That would have been my very first recommendation, wouldn't it be included in the code in your original post... This is why it's important to post always the current and complete version of code... ;) Glad you got it working. Jan