cancel
Showing results for 
Search instead for 
Did you mean: 

DMA Register Timer Input Capture STM32G431

pedahl
Associate II

Hi,

I would like to measure the times and pulse lengths of an external signal from a GPIO. For this I wanted to use a DMA trigger (which writes the time points from the Tim to the memory).
Here are 2 questions:
1. where can I find a document that states which DMA channel reads which register (generally for all registers and specifically for the timer)? (I have not found anything in the reference manual)
2. how can I trigger the DMA in the event of an edge?

Bests

Brian

1 REPLY 1
waclawek.jan
Super User

> which DMA channel reads which register

DMA channels can read from any address, as per their memory or peripheral address register (depending on direction). There may be consequences of reading some registers, same as when you read them from software (e.g. clearing status bits in hardware).

In your case, start with reading the TIM, DMAMUX and DMA chairs in RM. Set up Timer Capture in TIM, test, and if confident with that, wet up DMA triggered by the respective CCxF flag, to transfer the respective TIMx_CCRx to memory buffer. 

JW