2015-12-09 9:28 PM
I'm using STM32F4 discovery board and I'm receiving 38 bytes on UART RX line periodically, since I want to transfer this in DMA I used DMA circular mode.
But according to equation DMA_SxNDTR = Multiple of ((Mburst beat) � (Msize)/(Psize)), (Mburst beat) = 4, 8 or 16, ((Msize)/(Psize)) = 1, 2, 4, 1/2 or 1/4 My requirement wont satisfy the equation, so how can I configure the DMA in Circular mode for 38 bytes ? #dma #usart2015-12-09 10:02 PM
You did not mention the STM32 model you are using.
That remark, while probably valid when bursts set, is confusing indeed, as it appears to imply that there is no non-burst mode. There is. Just set MBURST to 00. Mayla or somebody else from ST, can you please command and/or initiate an appropriate amendment that comment? Thanks. JW2015-12-10 2:45 AM
Please don't modify posts after they have been answered.
I have given you the hint how to do it above - don't use bursts at all. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.