2024-01-31 8:36 AM - last edited on 2024-01-31 8:47 AM by mƎALLEm
Good afternoon,
I am developing an hardware with microcontroller in Object.
I'm using the LQFP208 package because in my opinion it's easier to solder/remove in my lab.
For my application I need the support for:
when I try to create the IOC file I have some problems with the FMC setting for the SDRAM.
All the peripherals end with the green check instead I have a warning on the FMC and so I don't understand whether or not I can use this processor with these requirements.
Anyone could help me?
Thanks in advance
Alfredo
Solved! Go to Solution.
2024-02-01 3:21 AM
Because you selected LTDC in DSI mode:
So select the line in the next indicated by an arrow.
2024-02-01 3:24 AM
Thanks