2024-11-12 10:51 AM - last edited on 2024-11-12 2:04 PM by Tesla DeLorean
where I wrote it among the codes.. // Here I have to wait 500ms.
Can you help me to prevent the timers from being affected by this wait?
Can you give me the codes that I will add. Because I am very confused..
I tried many things but they all stopped the interrupts..
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(htim->Instance==TIM1)
{
if(input1==0)
{
HAL_GPIO_WritePin(GPIOA, GPIO_Pin_1, GPIO_PIN_SET);
// Here I have to wait 500ms.
HAL_GPIO_WritePin(GPIOA, GPIO_Pin_1, GPIO_PIN_RESET);
}
}
Solved! Go to Solution.
2024-11-17 12:37 AM
You must not have read the last sentence in the Wiki? It says you need to add a call to TimerCallbacktick. You should have a file stm32fxxx_it.c in the src folder that has the SysTick_Handler
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
TimerCallbackTick(&timerCallback);
/* USER CODE END SysTick_IRQn 1 */
}Yes, the Timercallback.c/h can be used for any microcontroller. You're not limited to the Systick at 1ms.
You could also create a Timer interrupt for 100us and use both Timercallback instances, one for 1ms, and the other 100us.
2024-11-17 2:00 AM - edited 2024-11-17 2:00 AM
I guess I'm really ***. No matter what I do, it doesn't work.
TimerCallbackTimerStart(&timerCallback, PA10_Off, 500, TIMER_NO_REPEAT);
doesn't work..
PA10_off function doesn't work.
2024-11-17 7:20 AM
Does PA10 turn on?
Attach your project
2024-11-17 7:34 AM - edited 2024-11-17 10:08 AM
I couldn't do it with TimerCallback either
It didn't work like this either..
If PA2 is 0, PB14 should be 1 and PB14 should be 0 again for 500ms.
2024-11-17 9:01 AM
You uploaded the wrong project. It doesn't have the TimerCallback files.
2024-11-17 10:07 AM - edited 2024-11-17 10:43 PM
Eklediğimde hata verdi. Dosyaları kaldırdım. Onları ekleyebilir misiniz? Onları ekleyip size tekrar haber vermeli miyim?
Bu projeye eklediğimde çok fazla hata alıyorum.
Ekledim ama sorunları çözemedim.
2024-11-17 10:23 AM
If you removed the files then how am i supposed to see what errors occurred?
2024-11-17 2:16 PM
I added it in the message above and uploaded it again
2024-11-17 4:10 PM
Your project still looks the same. Your while loop is empty so not much is going to work.
Your project tree should look like this
You don't have GPIO set up correctly for the ones that use EXTI. Only the pins that you are polling use Input mode.
I highlighted from my IOC what it should be like.
The TimerCallback.c/h and PollingRoutine.c/h just drop in your project. The only thing you need to do is change the GPIO names i've used to the name you used.
2024-11-17 9:59 PM - edited 2024-11-17 11:10 PM