cancel
Showing results for 
Search instead for 
Did you mean: 

Debugging the Linux kernel

Rami Rosenbaum
Associate II

Hi,

I'm looking for a cheap board for debugging the Linux kernel, for a POC.

I thought of the stm32f429-disco. It is limited in resources, has no MMU/virtual-memory, but it's not a necessity for now.

I'm experienced with bare-metal stm32 programming, debugging the startup code from the reset-handler.

  1. Will I have these abilities when debugging the U-Boot/Kernel boot?
  2. Is the Linux environment up-to-date (kernel 4.X) and stable?
  3. Is setting up the bring-up environment straight-forward?

Thanks.

0 REPLIES 0