Debugging of my STEVAL-CCM001V2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-10-14 3:38 AM
Posted on October 14, 2013 at 12:38
Hello together,
I got an STEVAL-CCM001V2 evaluation board. This Board has an TFT-Display and some touch-keys to control the function of the board. The board has an micro-SD card slot and you could watch pictures on the sd-card over the usb-connection.When I got the board Iconnected it with my pc and after the driver was installed I could see the data on the card and watch pictures from the card on the board. Also I could configure the time and date in the menue, I would say basically the normal function.So in the package there is also the software of the application, and I have the ST-Link/V2 and I wanted to debug the application over SWD and my ST-LINK/V2.So I compiled direct the project from the CD and flashed it down into the controller and when I started it, the display was white an the usb-port is registered in the pc and after a few seconds the usb-port disappears in the pc.I think the software which is delivered with the package doesen't met to board or there is a new version which is different.If I could get the working programming file I could put the board in the delivered state but now it does not work anymore.Is there anybody who knows the board or has similar experiences?Thanks
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-10-14 4:53 AM
Posted on October 14, 2013 at 13:53
Should perhaps have used the ST-Link utilities to have saved the original firmware first? Maybe you can find some other user with the board? Not seeing much traffic in that regard.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..