Question
STM32F405 - No clock on SPI
Posted on October 14, 2013 at 11:27
Hello,
I've some problems with the SPI interface of the STM32F405 microcontroller. I hope someone could help me.I've a F-RAM connected to the STM32F405 via SPI. I'll checked pin connection and GPIO configuration with an oscilloscope ( set/reset IO), all works.But I'm not able to receive or transmit data with SPI interface. There is no clock generating on the Clock pin (PC10).
To my code : GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; SPI_I2S_DeInit( SPI3); /* Enable GPIO and SPI Periph Clock */ RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOA, ENABLE ); RCC_APB1PeriphClockCmd( RCC_APB1Periph_SPI3, ENABLE ); /* Connect CLK, MISO, MOSI and CS on AF6 */ GPIO_PinAFConfig( GPIOC, GPIO_Pin_10, GPIO_AF_SPI3 ); GPIO_PinAFConfig(GPIOC
,GPIO_Pin_11
, GPIO_AF_SPI3 ); GPIO_PinAFConfig(GPIOC
,GPIO_Pin_12
, GPIO_AF_SPI3 ); GPIO_PinAFConfig( GPIOA,GPIO_Pin_4
, GPIO_AF_SPI3 ); /* Configure SPI pins: ---------------------------------------------------*/ /* Configure SCK MISO and MOSI pins as Alternate Function Push Pull */ GPIO_InitStructure.GPIO_Pin =GPIO_Pin_10
|GPIO_Pin_11
|GPIO_Pin_12
; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_Init( GPIOC, &GPIO_InitStructure ); /* Configure CS pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_Init( GPIOA, &GPIO_InitStructure ); GPIO_SetBits( GPIOA,GPIO_Pin_4
); /* Configure Write Protection pin (active low) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_Init( GPIOB, &GPIO_InitStructure ); GPIO_SetBits(GPIOB
,GPIO_Pin_0
); /* SPI Configuration -----------------------------------------------------*/ SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init( SPI3, &SPI_InitStructure ); /* TEST */ /* Enable the SPI peripheral */ SPI_Cmd( SPI3, ENABLE ); /* Enable CS (active low) */ GPIO_ResetBits( GPIOA, GPIO_Pin_4); while( 1 ) { SPI_I2S_SendData( SPI3, 0xAA ); }Thanks & Best regards,Aurélie.