2022-01-03 09:40 PM
2022-01-03 11:13 PM
Welcome, @Karthik Kumar, to the community!
The file size of the HEX file is irrelevant, since it is a text file with additionally addresses, checksums, etc. Comparable with the Flash size would be only the BIN format.
So, don't worry, a HEX with 45KB perfectly fits into a 32KB Flash.
Regards
/Peter
2022-01-03 11:13 PM
Welcome, @Karthik Kumar, to the community!
The file size of the HEX file is irrelevant, since it is a text file with additionally addresses, checksums, etc. Comparable with the Flash size would be only the BIN format.
So, don't worry, a HEX with 45KB perfectly fits into a 32KB Flash.
Regards
/Peter
2022-01-04 12:07 AM
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Good luck!
/Peter
2022-01-04 12:07 AM
Dear Peter BENSCH
Thank you for you're response..
2022-03-06 10:02 PM
Hello @Peter BENSCH
I couldn't locate the hex file in my project folder. I can see the .elf file and .BIN file. Could you please help. I am using stm32f429zi on a Nucleo 144 board.
2022-03-06 11:17 PM
Your question has nothing to do with the original thread, so please create a new one.
Regards
/Peter