cancel
Showing results for 
Search instead for 
Did you mean: 

DAC and DMA with STM32L0 Nucleo

stephane239955
Associate II
Posted on October 13, 2015 at 18:20

Hello,

Newbee, I'm trying to generate sinewave at 1Khz using DAC and DMA on my STM32L0R53 Nucleo Board.

I'm using STM32CubeMx to initialise DAC and DMA but doesn't work.

Where can I find tutorial or sample code? Sample code delivered with STM32Cube_FW_L0_V1.1.0 are not based on STM32CubeMx, ioc files aren't included.

Thanks for your help

#dac #dma #stm32l053
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on October 28, 2015 at 15:09

Hi Steph,

I confirm that there is a plan to add *.ioc file for Projects under STM32Cube library but unfortunately not at the short term.

Where can I find tutorial or sample code? 

As you said STM32Cube_FW_L0_V1.3.0 provides projects that give description of how to use the DAC peripheral to generate several signals using DMA controller, you can start from it.

-Syrine-