2024-10-03 08:36 AM - edited 2024-10-03 08:40 AM
Hello,
VDD50USB on STM32H755II is powered from external 3.3V supply. What is the general use current consumption of the internal USB regulator?
Thanks!
Solved! Go to Solution.
2024-10-04 03:42 AM
Hi @drad1
VDD50USB can be supplied through the USB cable to generate the VDD33USB via the
USB internal regulator. The current consumed through the VDD50USB port on the STM32H755XI MCU is around 10mA.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-04 03:42 AM
Hi @drad1
VDD50USB can be supplied through the USB cable to generate the VDD33USB via the
USB internal regulator. The current consumed through the VDD50USB port on the STM32H755XI MCU is around 10mA.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.