2018-07-13 1:20 PM
Any one have any info on when cubemx support for stm32h750 might be available?
2018-10-04 1:06 PM
Hi @STOne-32 ,
Could you please confirm STM32H750 is a 743 variant as speculated earlier in the thread?
I am looking at the latest Reference manual "STM32H75x/74x and 750" (actual title) and Chapter 1.5 is not up to date. Therefore I am wondering, if we(my company) purchase 750 could we expect to get the same security features as 753?
ps: we are currently using 753- EVAL and looking forward to 753-EVAL2
Really hoping for clarity on this =)
Cheer
/Dimi
2018-10-04 1:57 PM
750 won't have HASH/CRYPT
The RM has all these parts sharing a common die ID and stepping.
2018-10-04 5:34 PM
Very interesting information, because according to the Chapter on RSS in the latest Reference manual, all three variants 74x 75x 750 are supporting SecureBoot.
How could 750 support RSS with SecureBoot without the CRYPT module for decrypting a signed firmware image?
I hope they don't imply using a SW decryption on the signed image.
Thanks for your input @Community member ! Definitely rising the importance of the question =)
2018-12-05 9:10 AM
>>Does the H7 Rev X support DSI functionality?
Affirmative