2015-04-22 02:27 PM
2015-04-24 10:20 AM
2015-04-28 03:26 PM
2015-04-29 06:30 AM
Hello Steve,
It happens that sometimes some files get set in ''access denied'' mode by EWARM preventing successful MX project generation. Trying to generate again usually works. Please let us know if you have identified some actions that leads systematically to the problem.2015-04-30 08:57 PM
2015-05-06 04:41 AM
I have same problem, too. Try to place your project into folder without spaces and international letters in name. It usually helps to me.
2015-05-18 09:18 AM
2015-05-28 06:20 AM
I have same problem, too....
2015-06-12 02:23 AM
I have the same problem:
STMCubeMX generates all the code necessary, except it doesn't create a ''EWARM'' directory (nor any content). If I create this myself and use IAR to set up a Project I can use the code generated. What gives? Edit: If I change the directory to a not so deep path it works! A nested path six directories deep doesn't, but two does.2015-11-16 09:55 AM
As for me, a looked toward filepath with spec characters/spaces. for the time CubeMX was installed, it worked good, but today refused to make a EWARM files for me. the reason was a russian-named folders, containing repository.
moving reps to simple-named folder had overcome the issue