2016-11-29 01:26 PM
Hello,
I like CubeMX and would like to suggest a feature for the report generator. I use Nucleo boards a lot for development and small projects and the support for it is really great, but I always have to look up the layout of the Nucleo headers. I usually end up on mbed.org like for the F401: https://developer.mbed.org/platforms/ST-Nucleo-F401RE/ And I was wondering if that would not be a great thing to have in the report generated by CubeMX, alongside the pin layout already there. I would suggest a layout similar to the mbed website with all the available ports + special functions, and also a extra column for the own pin label. Because the basic layout is the same for the Nucleo32/64/... a general image with some custom rendered text should do the trick. Maybe the information (like pin mapping) is also already available in CubeMX. The name/type of the Nucleo Board at least is already there. I am looking forward hearing from you. Sincerely Markus #feature-request2016-11-29 11:35 PM
Dear User,
Your request is reported internally to our CubeMx team. Thank you for fast feedback and for your contribution in the STM32 Community. All comments and suggestions are welcome to improve our solutions. Best Regards -Imen-