2017-10-17 10:04 AM
The code generated for an F303CCTx LL Active level Inversion of USART1 RX is :-
LL_USART_SetRXPinLevel(USART1, UART_ADVFEATURE_RXINV_ENABLE);
which doesn't compile. Where as I think it should be :-
LL_USART_SetRXPinLevel(USART1, LL_USART_RXPIN_LEVEL_INVERTED);The TX doesn't have this problem.
I also found that I need to add :-
/* Enable RXNE and Error interrupts */
LL_USART_EnableIT_RXNE(USART1); LL_USART_EnableIT_ERROR(USART1);to enable the interrupts I need. As it would seem the best place to add these is in the MX_USART1_UART_Init function that is generated, would it be possible to add a user code section at the end of the function to add this code to.
Solved! Go to Solution.
2018-02-08 5:50 AM
Hello
Fisher.David.003
,
Sorry for my late reply.
This issue is now solved. Please, update your CubeMX release with the current one (CubeMX-4.24).
BR. Jeanne
2017-10-20 5:16 AM
Hi,
Your reported issue is raised internally for further investigation.
Best Regards
Imen
2018-02-08 5:50 AM
Hello
Fisher.David.003
,
Sorry for my late reply.
This issue is now solved. Please, update your CubeMX release with the current one (CubeMX-4.24).
BR. Jeanne