cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.12

mrubinstein
Associate II
Posted on December 04, 2015 at 17:19

When will CubeMX 4.12 be available?

Thanks
2 REPLIES 2
hbarta2
Associate III
Posted on December 08, 2015 at 22:05

It's there now. http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF259242?sc=microxplorer

mrubinstein
Associate II
Posted on December 09, 2015 at 14:55

Thanks for the info.

I tried the new version and it works much better than 4.11.0.

4.11.0 made a mess of my existing IAR projects.

4.12.0 still required some cleanup, but it was not too bad:

  • It had a mixture of 1.3.0 and 1.4.0 #include search paths.
  • It included both the 1.3.0 and 1.4.0 versions of startup_xxx.s

I fixed up seven projects in less than an hour.  The best news is that everything seems to run fine on the target hardware.