cancel
Showing results for 
Search instead for 
Did you mean: 

Cube project generation and samples

John Davis_2
Associate II
Posted on April 03, 2017 at 21:22

I dont have much of a problem using the examples, but I do have a problem if I try to use ioc/cube generated samples that I try to retro fit in example code from the discovery repot.

In particular, the touch middleware is not provided by the cube software so I have to hand fit in the code from the example and then try to fix the gazillion errors.  Well not a gazillion, but 310 errors.  

Its not easy problem to solve with the headers included in headers.

1 REPLY 1
Imen.D
ST Employee
Posted on April 04, 2017 at 10:16

Hi

Davis.John.004

,

Your description of the issue is general.

You should identify what is the problem that you see and when it occurs.

Formore understand the issue you are facing, you can share your .ioc/code file and precisewhich device, firmware and CubeMx version you have used.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen