cancel
Showing results for 
Search instead for 
Did you mean: 

copying a dual-core project

YAtta.1
Associate

I have problem with duplicating an existing dual-core project in STM32CubeIDE. in single core project it was just sufficient to copy and paste a project to save it with another name. but for dual core project this doesnot work. hoe can we duplicate an existing dual-core project in STM32CubeIDE?

1 REPLY 1
'SMike
Associate III

This is also an issue when storing the project in git and cloning to another workspace. This is a very basic activity that should be supported.