Skip to main content
na_it
Associate II
November 9, 2021
Question

constant square wave on USART2_TX (PA2) after a power cycle (brown-out)

  • November 9, 2021
  • 32 replies
  • 9322 views

We get a constant square wave on USART2_TX (PA2) on some of our STM32L451CEU6TR products. This seems to happen sometimes after a power cycle (brown-out). The square wave is a around 32kHz.

 

As mentioned, this only happens on a few of our units, and after it has happened it doesn't seem to go away. It comes back after a power cycle event or a reset. One of the first thing we do, is to write on the UART, but we never see this, the oscillations starts before that (and the UART data will not come through after that). But the USART2_RX (PA3) still works. We can still send data to the MCU. The 32kHz isn't the same as the 32,768kHz. It's a little bit lower (like 31,9...). This was one of our thoughts that there had happened some HW changes inside the MCU so the RTC-clock was ported out here. But this doesn't seem to be the case.

This topic has been closed for replies.

32 replies

waclawek.jan
Super User
November 9, 2021

Can you connect with debugger? If yes, read out and check/post content of GPIOA_MODER/GPIOA_AFR and RCC_BDCR.

JW

na_it
na_itAuthor
Associate II
November 9, 2021

Sorry, but no. We can't connect a debugger. It's protected, so if we connect a debugger it will erase everything. We have our own debug-output on this UART....

Tesla DeLorean
Guru
November 9, 2021

Does your design pull BOOT0 low?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
na_it
na_itAuthor
Associate II
November 9, 2021

Boot0 is pulled low (by a 10k resistor).

waclawek.jan
Super User
November 9, 2021

Do you have a battery connected on VBAT? Do you have a 32.768kHz crystal connected and used as LSE?

Do you use Cube/HAL to initialize LSE and/or RTC? If yes, do you correctly set/clear *all* fields of the init struct before initializing LSE/RTC?

JW

na_it
na_itAuthor
Associate II
November 9, 2021

I'm using a PSU (tried with several different ones). The unit can be out of power for a long time, and when it starts up it starts to generate this wave again.

I'm not sure how this initilize is done (it's not me who have made it), but we suspect that it's not a SW thing. We have produced several 1000 of this PCB and we only see this on very few units. Units where the power have been cycled on/off for many times (mainly in our test system).

And yes, we have a 32,768kHz on the OSC32-pins. That was my first thought that it was that clock being routed to this pin, (for some strange reason), but it's not the same frequency. I can run a test-command and put out our 32,678 clock on another pin, so I measured both at the same time with the oscilloscope, and they differed.

waclawek.jan
Super User
November 9, 2021

> we suspect that it's not a SW thing

Show code which performs the LSE/RTC initialization.

> I can run a test-command and put out our 32,678 clock on another pin,

Using those test commands, can you read out RCC_BDCR somehow?

Or output LSI?

JW

S.Ma
Principal
November 10, 2021

Does your application meet all the stm32 electrical requirements respective to power up and sown supplies, slope, droops? What happen if you add say a 1 sec sw delay when the mcu is leaving low power mode? Is the pin configuration atomic in case or RTOS or gpio configured within interrupt/callback? Does the pin has MCO alternate on LSI ?

na_it
na_itAuthor
Associate II
November 10, 2021

Since we found out that, according to STM32 Application Note, LSCO can be output on PA2, it's safe to assume this is what we see. Question is, how can RCC_BDCR:LSCOEN suddenly be enabled? I don't think we ever touch this register except for setting RTCSEL and RTCEN, which we do via HAL/LL.

waclawek.jan
Super User
November 10, 2021

As I already wrote above: do you correctly set/clear *all* fields of the init struct before initializing LSE/RTC?

Post code.

JW

na_it
na_itAuthor
Associate II
November 10, 2021

static void hsiPllConfig(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct;

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLM = 2;

RCC_OscInitStruct.PLL.PLLN = 8;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;

RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;

RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

configASSERT(NULL);

}

}

static void lseConfig(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct;

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;

RCC_OscInitStruct.LSEState = RCC_LSE_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

configASSERT(NULL);

}

}

static void busClockConfig(void)

{

RCC_ClkInitTypeDef RCC_ClkInitStruct;

/**Initializes the CPU, AHB and APB busses clocks */

RCC_ClkInitStruct.ClockType

= RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

{

configASSERT(NULL);

}

}

static void SystemClock_Config(void)

{

RCC_PeriphCLKInitTypeDef PeriphClkInit;

/* Setup oscillators */

lseConfig();

hsiPllConfig();

/* Setup bus clocks */

busClockConfig();

/* Setup peripheral clocks */

PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC | RCC_PERIPHCLK_USART1

| RCC_PERIPHCLK_LPUART1 | RCC_PERIPHCLK_USART2

| RCC_PERIPHCLK_I2C1 | RCC_PERIPHCLK_I2C2

| RCC_PERIPHCLK_ADC | RCC_PERIPHCLK_LPTIM1;

PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;

PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_HSI;

PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;

PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;

PeriphClkInit.I2c2ClockSelection = RCC_I2C2CLKSOURCE_PCLK1;

PeriphClkInit.AdcClockSelection = RCC_ADCCLKSOURCE_SYSCLK;

PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;

PeriphClkInit.Lptim1ClockSelection = RCC_LPTIM1CLKSOURCE_LSE;

if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

{

configASSERT(NULL);

}

...}

Bob S
Super User
November 10, 2021

To make SURE that all structure elements are initialized (as @Community member​ mentioned), change your structure declarations in your clock fonfig functions from this:

RCC_OscInitTypeDef RCC_OscInitStruct;

to this:

RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };

This guarantees that and member you don't explicitly init gets set to zero. Otherwise it contains somewhat random data, depending on the stack contents.

Tesla DeLorean
Guru
November 10, 2021

This

Failure to initialize auto/local variables properly, especially large structures ST is apt to using is a primary cause of undefined/indeterminate operation.

They've caught this on a lot of the examples/autogens, but it's one of those gifts that keeps giving.

They can get away with it with globals as the C run-time library has a contract to clear them and initialize the statics during startup.

#SituationalAwareness

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
November 10, 2021

While BobS is generally right, in this particular case, I went through relevant functions in current CubeL4 I can't see anything problematic there... I am out of ideas, sorry.

You should first try to confirm as much as possible that this is indeed related to RCC_BDCR.LSCOEN. On an affected system, perform backup domain reset, i.e. remove *both* VDD *and* the backup battery from VBAT; after placing them back the issue should go away.

Then you should try to reproduce the problem on an "unlocked" development version of the device, while having a data breakpoint (watchpoint) set on RCC_BDCR so you can catch the code which caused the problem.

Bat keep your mind open - there's still chance that this is something else and we just misinterpret the symptoms.

I know this is not simple. Sorry I cannot help more.

JW

Eis
Visitor II
November 11, 2021

Thank you all for good advice,

I'm fully aware about the uninitialized struct parts, but checking the code all relevant fields were initialized ok, so I guess we're happy with that.

At least we found out (most likely) what is actually causing the problem. We've already verified that removing all power from both VDD and VBAT "solves" the problem. We will continue to investigate the root-cause of the problem.